RoutingPathOccChainable Enumeration

NXOpen.Preferences.RoutingPath.OccChainable is an alias for NXOpen.Preferences.RoutingPathOccChainable

class NXOpen.Preferences.RoutingPathOccChainable

Bases: object

Chain occurrences of curves ? [i.

  1. curves not in the work part]

Enum Members

Enum Member Enum Member Description
False
True
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.