RoutingPathMergeDupRcps Enumeration

NXOpen.Preferences.RoutingPath.MergeDupRcps is an alias for NXOpen.Preferences.RoutingPathMergeDupRcps

class NXOpen.Preferences.RoutingPathMergeDupRcps

Bases: object

Should duplicate RCPs be merged after a Transform [Move or Copy] operation?

Enum Members

Enum Member Enum Member Description
False
Do not merge duplicate RCPs.
True
Merge duplicate RCPs.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.