RoutingPathCurveType Enumeration¶
NXOpen.Preferences.RoutingPath.CurveType is an alias for NXOpen.Preferences.RoutingPathCurveType
-
class
NXOpen.Preferences.
RoutingPathCurveType
¶ Bases:
object
Describes the types of curves allowed in a routing application.
Enum Members
Enum Member Enum Member Description Line UF_ROUTE_AV_CURVES_LINESArc UF_ROUTE_AV_CURVES_ARCSSpline UF_ROUTE_AV_CURVES_SPLINES-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-