RoutingPathConfirmBranchSel Enumeration

NXOpen.Preferences.RoutingPath.ConfirmBranchSel is an alias for NXOpen.Preferences.RoutingPathConfirmBranchSel

class NXOpen.Preferences.RoutingPathConfirmBranchSel

Bases: object

Should a branch selection confirmation dialog be show during Path selection?

Enum Members

Enum Member Enum Member Description
False
Do not confirm branch selection.
True
Confirm branch selection.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.