RoutingPathChainMethod Enumeration

NXOpen.Preferences.RoutingPath.ChainMethod is an alias for NXOpen.Preferences.RoutingPathChainMethod

class NXOpen.Preferences.RoutingPathChainMethod

Bases: object

Path curve chaining methods

Enum Members

Enum Member Enum Member Description
NoBranch
Curves must be mono-connected
Continuous
Tangents must match at each connection
Tangent
Use curve with closest tangent when searching
Cycle
Return all chains
MinDist
Chain with minimum path length
MaxDist
Chain with maximum path length
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.