RoutingLogicalFlowArrowEnumType Enumeration

NXOpen.Preferences.RoutingLogical.FlowArrowEnumType is an alias for NXOpen.Preferences.RoutingLogicalFlowArrowEnumType

class NXOpen.Preferences.RoutingLogicalFlowArrowEnumType

Bases: object

How to create terminal segments (if creating terminal segments).

Enum Members

Enum Member Enum Member Description
Open
Open arrow head on flow arrow.
Closed
Closed arrow head on flow arrow.
Filled
Filled arrow head on flow arrow.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.