RoutingElectricalCreateTerminalsType Enumeration

NXOpen.Preferences.RoutingElectrical.CreateTerminalsType is an alias for NXOpen.Preferences.RoutingElectricalCreateTerminalsType

class NXOpen.Preferences.RoutingElectricalCreateTerminalsType

Bases: object

How to create terminal segments (if creating terminal segments).

Enum Members

Enum Member Enum Member Description
All
Create terminals to all terminals
Listed
Create terminals to listed terminals
Routed
Create terminals to routed terminals
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.