PartVisualizationShadeViewUpdateModeType Enumeration¶
NXOpen.Preferences.PartVisualizationShade.ViewUpdateModeType is an alias for NXOpen.Preferences.PartVisualizationShadeViewUpdateModeType
-
class
NXOpen.Preferences.
PartVisualizationShadeViewUpdateModeType
¶ Bases:
object
Describes whether the applied changes are applicable to visible object or all object or no object
Enum Members
Enum Member Enum Member Description VisibleObject Applicable only to visible objectAllObject Applicable to all objectNotSet No object-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-