PartVisualizationShadeShadedFaceEdge Enumeration

NXOpen.Preferences.PartVisualizationShade.ShadedFaceEdge is an alias for NXOpen.Preferences.PartVisualizationShadeShadedFaceEdge

class NXOpen.Preferences.PartVisualizationShadeShadedFaceEdge

Bases: object

Describes whether the shaded face edges are having no color or body color or user defined color.

Enum Members

Enum Member Enum Member Description
Off
Option is off
BodyColor
Body Color
SpecifyColor
Specified Color
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.