PartVisualizationShadeHiddenShadedFaceEdges Enumeration

NXOpen.Preferences.PartVisualizationShade.HiddenShadedFaceEdges is an alias for NXOpen.Preferences.PartVisualizationShadeHiddenShadedFaceEdges

class NXOpen.Preferences.PartVisualizationShadeHiddenShadedFaceEdges

Bases: object

Describes whether the shaded face edges are invisible or dashed visible or with a color to depict the hidden geometry

Enum Members

hidden are not displayed “
“Dashed”, ” If selected, hidden shaded face edges are

displayed in the body color with a dashed line font. “

“HiddenColor”, ” If any color is selected, hidden shaded face

edges are displayed in that color.”

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.