PartVisualizationShadeAdvViewToleranceType Enumeration¶
NXOpen.Preferences.PartVisualizationShade.AdvViewToleranceType is an alias for NXOpen.Preferences.PartVisualizationShadeAdvViewToleranceType
-
class
NXOpen.Preferences.
PartVisualizationShadeAdvViewToleranceType
¶ Bases:
object
Describes the available tolerance types for Advanced View.
Each of these options maps tolerance values to for specific operations : Curve Edge Chord Distance, Surface Chord Distance, Angular Tolerance, Facet Width Tolerance
Enum Members
Face Tolerance and Angle Tolerance, Width Tolerance specifically. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-