PartVisualizationPerformance Class

class NXOpen.Preferences.PartVisualizationPerformance

Bases: object

Represents the set of visualization performance preferences applicable to entire part.

To obtain an instance of this class, refer to NXOpen.Preferences.PartPreferences

New in version NX10.0.0.

Properties

Property Description
SaveAdvancedDisplayFacets Returns or sets the save advanced facets.

Methods

Property Detail

SaveAdvancedDisplayFacets

PartVisualizationPerformance.SaveAdvancedDisplayFacets

Returns or sets the save advanced facets.

Enable saving of advanced display facets in the part file.

-------------------------------------

Getter Method

Signature SaveAdvancedDisplayFacets()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SaveAdvancedDisplayFacets(saveAdvancedDisplayFacets)

Parameters:saveAdvancedDisplayFacets (bool) –

New in version NX10.0.0.

License requirements: None.