PartVisualizationNamesBorders Class

class NXOpen.Preferences.PartVisualizationNamesBorders

Bases: object

Represents the set of visualization preferences of entire Working Part coming under Names/borders Tab

To obtain an instance of this class, refer to NXOpen.Preferences.PartPreferences

New in version NX3.0.0.

Properties

Property Description
CharacterSize Returns or sets the character size.
ObjectNameDisplay Returns or sets the object name display
ShowModelViewBorders Returns or sets the show model view border flag.
ShowModelViewNames Returns or sets the show model view names flag.

Methods

Enumerations

PartVisualizationNamesBordersNameDisplay Enumeration Describes the available options for object name display selection

Property Detail

CharacterSize

PartVisualizationNamesBorders.CharacterSize

Returns or sets the character size.

Allows to define the size of the text in the object names

-------------------------------------

Getter Method

Signature CharacterSize()

Returns:
Return type:float

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CharacterSize(characterSize)

Parameters:characterSize (float) –

New in version NX3.0.0.

License requirements: None.

ObjectNameDisplay

PartVisualizationNamesBorders.ObjectNameDisplay

Returns or sets the object name display

-------------------------------------

Getter Method

Signature ObjectNameDisplay()

Returns:
Return type:NXOpen.Preferences.PartVisualizationNamesBordersNameDisplay

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ObjectNameDisplay(objectNameDisplay)

Parameters:objectNameDisplay (NXOpen.Preferences.PartVisualizationNamesBordersNameDisplay) –

New in version NX3.0.0.

License requirements: None.

ShowModelViewBorders

PartVisualizationNamesBorders.ShowModelViewBorders

Returns or sets the show model view border flag.

allows to turn on and off the display of view borders.

-------------------------------------

Getter Method

Signature ShowModelViewBorders()

Returns:
Return type:bool

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowModelViewBorders(showModelViewBorders)

Parameters:showModelViewBorders (bool) –

New in version NX3.0.0.

License requirements: None.

ShowModelViewNames

PartVisualizationNamesBorders.ShowModelViewNames

Returns or sets the show model view names flag.

Allows to turn on and off the display of view names.

-------------------------------------

Getter Method

Signature ShowModelViewNames()

Returns:
Return type:bool

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowModelViewNames(showModelViewNames)

Parameters:showModelViewNames (bool) –

New in version NX3.0.0.

License requirements: None.