PartModelingDensityUnitType Enumeration¶
NXOpen.Preferences.PartModeling.DensityUnitType is an alias for NXOpen.Preferences.PartModelingDensityUnitType
-
class
NXOpen.Preferences.
PartModelingDensityUnitType
¶ Bases:
object
Describes the units available for representing density
Enum Members
Enum Member Enum Member Description LbPerCuInch Unit is pound per cubic inchLbPerCuFeet Unit is pound per cubic feetGmPerCuCm Unit is gram per cubic centimeterKgPerCuMeter Unit is kg per cubic meter-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-