PartModelingCurveCurvatureDisplayType Enumeration¶
NXOpen.Preferences.PartModeling.CurveCurvatureDisplayType is an alias for NXOpen.Preferences.PartModelingCurveCurvatureDisplayType
-
class
NXOpen.Preferences.
PartModelingCurveCurvatureDisplayType
¶ Bases:
object
Describes whether the curve curvature display is Curvature Comb or radius of Curvature Comb
Enum Members
Enum Member Enum Member Description Comb Curve curvature display is Curvature CombRadiusOfComb Curve curvature display is radius of Curvature Comb-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-