PartFlexiblePrintedCircuitDesign Class¶
-
class
NXOpen.Preferences.
PartFlexiblePrintedCircuitDesign
¶ Bases:
object
Represents the Flexible Printed Circuit Design preferences applicable to part
Preferences are in control of the part. They can not be created but can only be changed.
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits and applies all the settings done with set_callout_type_display and set_object_type_display. |
GetBendRadius | Returns the bend radius expression @return expression object for radius of bend faces |
GetBendReliefDepth | Returns the bend relief depth @return expression object for depth of bend relief |
GetBendReliefWidth | Returns the bend relief width @return expression object for width of bend relief |
GetDeviationalToleranceInFlatSolid | Returns the deviational tolerance during Flat Solid simplification @return flag |
GetFlatPatternAllCalloutTypeDisplay | Returns the dialog names, identifiers, and enabled status for all the available callout types. |
GetFlatPatternAllObjectTypeDisplay | Returns the types, colors, fonts, widths, and enabled status for all the the available object types. |
GetFlatPatternCalloutOrientationType | Returns the orientation type for flat pattern callouts. |
GetFlatPatternCalloutTypeContents | Returns the contents for a callout type. |
GetFlatPatternCalloutTypeDisplay | Returns the display data for a callout type. |
GetFlatPatternObjectTypeDisplay | Returns the display data for a flat pattern object type. |
GetFlexibleCableBottomFaceColor | Returns the bottom face color. |
GetFlexibleCableConductorSpacing | Returns the conductor spacing expression. |
GetFlexibleCableConductorWidth | Returns the conductor width expression. |
GetFlexibleCableContactFace | Returns the contact face. |
GetFlexibleCableStrippingLength | Returns the stripping length expression. |
GetFlexibleCableTopFaceColor | Returns the top face color. |
GetInnerCornerTreatmentType | Returns the inner corner treatment type in Flat as Solid operation @return outer corner treatment type |
GetInnerCornerTreatmentValue | Returns the inner corner treatment value for Flat as Solid operations @return expression object for inner corner treatment value |
GetIsBsplineSimplifiedInFlatSolid | Returns the flag indicating whether B-Splines are simplified as part of the Flat Solid creation @return flag |
GetIsSystemGeneratedBendReliefRemovedInFlatSolid | Returns the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation @return flag |
GetMaterial | Returns the material name saved with the part @return The name of the material saved with the part |
GetMaterialNames | Returns the material names defined in the material standards table @return |
GetMaterialProperties | Returns the material name saved with the part @return property Values |
GetMinimumArcToleranceInFlatSolid | Returns the minimum arc tolerance during Flat Solid simplification @return flag |
GetNeutralFactor | Returns the neutral factor @return expression object for neutral factor of bend areas |
GetOuterCornerTreatmentType | Returns the outer corner treatment type in Flat as Solid operation @return outer corner treatment type |
GetOuterCornerTreatmentValue | Returns the out corner treatment value for Flat as Solid operations @return expression object for out corner treatment value |
GetThickness | Returns the thickness expression @return expression object for sheet thickness |
SetBendRadius | Sets the bend radius value |
SetBendReliefDepth | Sets the bend relief depth value |
SetBendReliefWidth | Sets the bend relief depth value |
SetDeviationalToleranceInFlatSolid | Sets the deviational tolerance during Flat Solid simplification |
SetFlatPatternCalloutOrientationType | Sets the orientation type for flat pattern callouts. |
SetFlatPatternCalloutTypeContents | Sets the contents for a callout type. |
SetFlatPatternCalloutTypeDisplay | Sets the display data for a callout type. |
SetFlatPatternObjectTypeDisplay | Sets the display data for a flat pattern object type. |
SetFlexibleCableBottomFaceColor | Sets the bottom face color. |
SetFlexibleCableConductorSpacing | Sets the conductor spacing value string. |
SetFlexibleCableConductorWidth | Sets the conductor width value string. |
SetFlexibleCableContactFace | Sets the contact face. |
SetFlexibleCableStrippingLength | Sets the stripping length value string. |
SetFlexibleCableTopFaceColor | Sets the top face color. |
SetInnerCornerTreatmentType | Sets the inner corner treatment type in Flat as Solid operation |
SetInnerCornerTreatmentValue | Sets the the inner corner treatment value for Flat as Solid operations |
SetIsBsplineSimplifiedInFlatSolid | Sets the flag indicating whether or not B-Splines are simplified as part of the Flat Solid creation |
SetIsSystemGeneratedBendReliefRemovedInFlatSolid | Sets the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation |
SetMaterial | Sets the material standard |
SetMinimumArcToleranceInFlatSolid | Sets the minimum arc tolerance during Flat Solid simplification |
SetNeutralFactor | Sets the bend relief depth value |
SetOuterCornerTreatmentType | Sets the the outer corner treatment type in Flat as Solid operation |
SetOuterCornerTreatmentValue | Sets the outer corner treatment value for Flat as Solid operations |
SetThickness | Sets the thickness value string |
Enumerations¶
PartFlexiblePrintedCircuitDesignFlatPatternCalloutOrientationType Enumeration | This enum represents orientation types for the flat pattern callouts |
PartFlexiblePrintedCircuitDesignFlatPatternObjectType Enumeration | The members of the following enumerated type are used to identify object types to the FlatPattern API. |
PartFlexiblePrintedCircuitDesignFlexibleCableContactFaceOptions Enumeration | This enum represents the face that is the contact face of the Flexible Cable. |
Structs¶
PartFlexiblePrintedCircuitDesignFlatPatternCalloutTypeDisplay_Struct Struct | The members of the following structure are the display data for a callout in a flat pattern drawing member view. |
PartFlexiblePrintedCircuitDesignFlatPatternObjectTypeDisplay_Struct Struct | The members of the following structure are the display data for an object in a flat pattern drawing member view. |
Method Detail¶
Commit¶
-
PartFlexiblePrintedCircuitDesign.
Commit
¶ Commits and applies all the settings done with set_callout_type_display and set_object_type_display.
It must be called after a sequence of calls to those methods to cause the view to update.
Signature
Commit()
New in version NX5.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetBendRadius¶
-
PartFlexiblePrintedCircuitDesign.
GetBendRadius
¶ Returns the bend radius expression
Signature
GetBendRadius()
Returns: expression object for radius of bend faces Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetBendReliefDepth¶
-
PartFlexiblePrintedCircuitDesign.
GetBendReliefDepth
¶ Returns the bend relief depth
Signature
GetBendReliefDepth()
Returns: expression object for depth of bend relief Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetBendReliefWidth¶
-
PartFlexiblePrintedCircuitDesign.
GetBendReliefWidth
¶ Returns the bend relief width
Signature
GetBendReliefWidth()
Returns: expression object for width of bend relief Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetDeviationalToleranceInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
GetDeviationalToleranceInFlatSolid
¶ Returns the deviational tolerance during Flat Solid simplification
Signature
GetDeviationalToleranceInFlatSolid()
Returns: flag Return type: float New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlatPatternAllCalloutTypeDisplay¶
-
PartFlexiblePrintedCircuitDesign.
GetFlatPatternAllCalloutTypeDisplay
¶ Returns the dialog names, identifiers, and enabled status for all the available callout types.
Signature
GetFlatPatternAllCalloutTypeDisplay()
Returns: Array of structures with the callout type display data. Return type: list of NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternCalloutTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlatPatternAllObjectTypeDisplay¶
-
PartFlexiblePrintedCircuitDesign.
GetFlatPatternAllObjectTypeDisplay
¶ Returns the types, colors, fonts, widths, and enabled status for all the the available object types.
Signature
GetFlatPatternAllObjectTypeDisplay()
Returns: Array of structures with the object type display data. Return type: list of NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternObjectTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlatPatternCalloutOrientationType¶
-
PartFlexiblePrintedCircuitDesign.
GetFlatPatternCalloutOrientationType
¶ Returns the orientation type for flat pattern callouts.
Signature
GetFlatPatternCalloutOrientationType()
Returns: The orientation type for the flat pattern callouts. Return type: NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternCalloutOrientationType
New in version NX9.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlatPatternCalloutTypeContents¶
-
PartFlexiblePrintedCircuitDesign.
GetFlatPatternCalloutTypeContents
¶ Returns the contents for a callout type.
Signature
GetFlatPatternCalloutTypeContents(calloutType)
Parameters: calloutType (str) – The name of the callout type for which to get the content. Returns: The contents for the callout type. Return type: list of str New in version NX9.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlatPatternCalloutTypeDisplay¶
-
PartFlexiblePrintedCircuitDesign.
GetFlatPatternCalloutTypeDisplay
¶ Returns the display data for a callout type.
The name member of the
NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternCalloutTypeDisplay_Struct
is separately allocated from the callout_type argument string. In some cases the new string will contain an extended form of the callout_type passed in, and that form should be used for subsequent JA calls, without modification.Signature
GetFlatPatternCalloutTypeDisplay(calloutType)
Parameters: calloutType (str) – The name of the callout type for which to get the display data. Returns: The display data for the callout type. Return type: NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternCalloutTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlatPatternObjectTypeDisplay¶
-
PartFlexiblePrintedCircuitDesign.
GetFlatPatternObjectTypeDisplay
¶ Returns the display data for a flat pattern object type.
Signature
GetFlatPatternObjectTypeDisplay(objectType)
Parameters: objectType ( NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternObjectType
) – The object type for which to return the display data.Returns: The display data for the flat pattern object type. Return type: NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternObjectTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlexibleCableBottomFaceColor¶
GetFlexibleCableConductorSpacing¶
-
PartFlexiblePrintedCircuitDesign.
GetFlexibleCableConductorSpacing
¶ Returns the conductor spacing expression.
Signature
GetFlexibleCableConductorSpacing()
Returns: expression object for flexible cable conductor width. Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlexibleCableConductorWidth¶
-
PartFlexiblePrintedCircuitDesign.
GetFlexibleCableConductorWidth
¶ Returns the conductor width expression.
Signature
GetFlexibleCableConductorWidth()
Returns: expression object for flexible cable conductor width. Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlexibleCableContactFace¶
-
PartFlexiblePrintedCircuitDesign.
GetFlexibleCableContactFace
¶ Returns the contact face.
Signature
GetFlexibleCableContactFace()
Returns: Return type: NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlexibleCableContactFaceOptions
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlexibleCableStrippingLength¶
-
PartFlexiblePrintedCircuitDesign.
GetFlexibleCableStrippingLength
¶ Returns the stripping length expression.
Signature
GetFlexibleCableStrippingLength()
Returns: expression object for flexible cable conductor width. Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetFlexibleCableTopFaceColor¶
GetInnerCornerTreatmentType¶
-
PartFlexiblePrintedCircuitDesign.
GetInnerCornerTreatmentType
¶ Returns the inner corner treatment type in Flat as Solid operation
Signature
GetInnerCornerTreatmentType()
Returns: outer corner treatment type Return type: NXOpen.Features.SheetMetal.FeatureProperty
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetInnerCornerTreatmentValue¶
-
PartFlexiblePrintedCircuitDesign.
GetInnerCornerTreatmentValue
¶ Returns the inner corner treatment value for Flat as Solid operations
Signature
GetInnerCornerTreatmentValue()
Returns: expression object for inner corner treatment value Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetIsBsplineSimplifiedInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
GetIsBsplineSimplifiedInFlatSolid
¶ Returns the flag indicating whether B-Splines are simplified as part of the Flat Solid creation
Signature
GetIsBsplineSimplifiedInFlatSolid()
Returns: flag Return type: bool New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetIsSystemGeneratedBendReliefRemovedInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
GetIsSystemGeneratedBendReliefRemovedInFlatSolid
¶ Returns the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation
Signature
GetIsSystemGeneratedBendReliefRemovedInFlatSolid()
Returns: flag Return type: bool New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetMaterial¶
-
PartFlexiblePrintedCircuitDesign.
GetMaterial
¶ Returns the material name saved with the part
Signature
GetMaterial()
Returns: The name of the material saved with the part Return type: str New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetMaterialNames¶
-
PartFlexiblePrintedCircuitDesign.
GetMaterialNames
¶ Returns the material names defined in the material standards table
Signature
GetMaterialNames()
Returns: Return type: list of str New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetMaterialProperties¶
-
PartFlexiblePrintedCircuitDesign.
GetMaterialProperties
¶ Returns the material name saved with the part
Signature
GetMaterialProperties(materialName)
Parameters: materialName (str) – material Name Returns: a tuple Return type: A tuple consisting of (propertyValues, propertyNames). propertyValues is a list of str. property Values propertyNames is a list of str. properties New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetMinimumArcToleranceInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
GetMinimumArcToleranceInFlatSolid
¶ Returns the minimum arc tolerance during Flat Solid simplification
Signature
GetMinimumArcToleranceInFlatSolid()
Returns: flag Return type: float New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetNeutralFactor¶
-
PartFlexiblePrintedCircuitDesign.
GetNeutralFactor
¶ Returns the neutral factor
Signature
GetNeutralFactor()
Returns: expression object for neutral factor of bend areas Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetOuterCornerTreatmentType¶
-
PartFlexiblePrintedCircuitDesign.
GetOuterCornerTreatmentType
¶ Returns the outer corner treatment type in Flat as Solid operation
Signature
GetOuterCornerTreatmentType()
Returns: outer corner treatment type Return type: NXOpen.Features.SheetMetal.FeatureProperty
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetOuterCornerTreatmentValue¶
-
PartFlexiblePrintedCircuitDesign.
GetOuterCornerTreatmentValue
¶ Returns the out corner treatment value for Flat as Solid operations
Signature
GetOuterCornerTreatmentValue()
Returns: expression object for out corner treatment value Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
GetThickness¶
-
PartFlexiblePrintedCircuitDesign.
GetThickness
¶ Returns the thickness expression
Signature
GetThickness()
Returns: expression object for sheet thickness Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetBendRadius¶
-
PartFlexiblePrintedCircuitDesign.
SetBendRadius
¶ Sets the bend radius value
Signature
SetBendRadius(updateModel, bendRadius)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendRadius (str) – default bend radius value for bend faces
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetBendReliefDepth¶
-
PartFlexiblePrintedCircuitDesign.
SetBendReliefDepth
¶ Sets the bend relief depth value
Signature
SetBendReliefDepth(updateModel, bendReliefDepth)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendReliefDepth (str) – default depth value for bend relief
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetBendReliefWidth¶
-
PartFlexiblePrintedCircuitDesign.
SetBendReliefWidth
¶ Sets the bend relief depth value
Signature
SetBendReliefWidth(updateModel, bendReliefWidth)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendReliefWidth (str) – default width value for bend relief
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetDeviationalToleranceInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
SetDeviationalToleranceInFlatSolid
¶ Sets the deviational tolerance during Flat Solid simplification
Signature
SetDeviationalToleranceInFlatSolid(updateModel, deviationalToleranceInFlatSolid)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- deviationalToleranceInFlatSolid (float) – flag
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlatPatternCalloutOrientationType¶
-
PartFlexiblePrintedCircuitDesign.
SetFlatPatternCalloutOrientationType
¶ Sets the orientation type for flat pattern callouts.
Signature
SetFlatPatternCalloutOrientationType(orientation)
Parameters: orientation ( NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternCalloutOrientationType
) – The orientation type for the flat pattern callouts.New in version NX9.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlatPatternCalloutTypeContents¶
-
PartFlexiblePrintedCircuitDesign.
SetFlatPatternCalloutTypeContents
¶ Sets the contents for a callout type.
Signature
SetFlatPatternCalloutTypeContents(calloutType, contents)
Parameters: - calloutType (str) – The name of the callout type for which to set the content.
- contents (list of str) – The contents for the callout type.
New in version NX9.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlatPatternCalloutTypeDisplay¶
-
PartFlexiblePrintedCircuitDesign.
SetFlatPatternCalloutTypeDisplay
¶ Sets the display data for a callout type.
Signature
SetFlatPatternCalloutTypeDisplay(calloutType, displayData)
Parameters: - calloutType (str) – The name of the callout type for which to set the display data.
- displayData (
NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternCalloutTypeDisplay_Struct
) – The display data for the callout type.
New in version NX5.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlatPatternObjectTypeDisplay¶
-
PartFlexiblePrintedCircuitDesign.
SetFlatPatternObjectTypeDisplay
¶ Sets the display data for a flat pattern object type.
Signature
SetFlatPatternObjectTypeDisplay(updateModel, objectType, displayData)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately.
- objectType (
NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternObjectType
) – The object type for which to get the display data. - displayData (
NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternObjectTypeDisplay_Struct
) – The display data for the flat pattern object type.
New in version NX5.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlexibleCableBottomFaceColor¶
SetFlexibleCableConductorSpacing¶
-
PartFlexiblePrintedCircuitDesign.
SetFlexibleCableConductorSpacing
¶ Sets the conductor spacing value string.
Signature
SetFlexibleCableConductorSpacing(conductorSpacing)
Parameters: conductorSpacing (str) – Default conductor spacing value for the flexible cable. New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlexibleCableConductorWidth¶
-
PartFlexiblePrintedCircuitDesign.
SetFlexibleCableConductorWidth
¶ Sets the conductor width value string.
Signature
SetFlexibleCableConductorWidth(conductorWidth)
Parameters: conductorWidth (str) – Default conductor width value for the flexible cable. New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlexibleCableContactFace¶
-
PartFlexiblePrintedCircuitDesign.
SetFlexibleCableContactFace
¶ Sets the contact face.
Signature
SetFlexibleCableContactFace(faceOption)
Parameters: faceOption ( NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlexibleCableContactFaceOptions
) – Contact face options.New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlexibleCableStrippingLength¶
-
PartFlexiblePrintedCircuitDesign.
SetFlexibleCableStrippingLength
¶ Sets the stripping length value string.
Signature
SetFlexibleCableStrippingLength(strippingLength)
Parameters: strippingLength (str) – Default stripping length value for the flexible cable. New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetFlexibleCableTopFaceColor¶
SetInnerCornerTreatmentType¶
-
PartFlexiblePrintedCircuitDesign.
SetInnerCornerTreatmentType
¶ Sets the inner corner treatment type in Flat as Solid operation
Signature
SetInnerCornerTreatmentType(updateModel, innerCornerTreatmentType)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- innerCornerTreatmentType (
NXOpen.Features.SheetMetal.FeatureProperty
) – outer corner treatment type
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetInnerCornerTreatmentValue¶
-
PartFlexiblePrintedCircuitDesign.
SetInnerCornerTreatmentValue
¶ Sets the the inner corner treatment value for Flat as Solid operations
Signature
SetInnerCornerTreatmentValue(updateModel, innerCornerTreatment)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- innerCornerTreatment (str) – default value for inner corner treatment
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetIsBsplineSimplifiedInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
SetIsBsplineSimplifiedInFlatSolid
¶ Sets the flag indicating whether or not B-Splines are simplified as part of the Flat Solid creation
Signature
SetIsBsplineSimplifiedInFlatSolid(updateModel, isBsplineSimplifiedInFlatSolid)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- isBsplineSimplifiedInFlatSolid (bool) – flag
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetIsSystemGeneratedBendReliefRemovedInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
SetIsSystemGeneratedBendReliefRemovedInFlatSolid
¶ Sets the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation
Signature
SetIsSystemGeneratedBendReliefRemovedInFlatSolid(updateModel, isSystemGeneratedBendReliefRemoved)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- isSystemGeneratedBendReliefRemoved (bool) – flag
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetMaterial¶
-
PartFlexiblePrintedCircuitDesign.
SetMaterial
¶ Sets the material standard
Signature
SetMaterial(updateModel, standardName)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- standardName (str) – The name of a material from the material standards file
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetMinimumArcToleranceInFlatSolid¶
-
PartFlexiblePrintedCircuitDesign.
SetMinimumArcToleranceInFlatSolid
¶ Sets the minimum arc tolerance during Flat Solid simplification
Signature
SetMinimumArcToleranceInFlatSolid(updateModel, minimumArcToleranceInFlatSolid)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- minimumArcToleranceInFlatSolid (float) – flag
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetNeutralFactor¶
-
PartFlexiblePrintedCircuitDesign.
SetNeutralFactor
¶ Sets the bend relief depth value
Signature
SetNeutralFactor(updateModel, neutralFactor)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- neutralFactor (str) – default neutral factor value for bend relief
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetOuterCornerTreatmentType¶
-
PartFlexiblePrintedCircuitDesign.
SetOuterCornerTreatmentType
¶ Sets the the outer corner treatment type in Flat as Solid operation
Signature
SetOuterCornerTreatmentType(updateModel, outerCornerTreatmentType)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- outerCornerTreatmentType (
NXOpen.Features.SheetMetal.FeatureProperty
) – outer corner treatment type
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetOuterCornerTreatmentValue¶
-
PartFlexiblePrintedCircuitDesign.
SetOuterCornerTreatmentValue
¶ Sets the outer corner treatment value for Flat as Solid operations
Signature
SetOuterCornerTreatmentValue(updateModel, outerCornerTreatment)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- outerCornerTreatment (str) – default value for out corner treatment
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
SetThickness¶
-
PartFlexiblePrintedCircuitDesign.
SetThickness
¶ Sets the thickness value string
Signature
SetThickness(updateModel, thickness)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- thickness (str) – default thickness value for NX Sheetmetal solids
New in version NX4.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)