PartDraftingUpdateViewWithoutLwDataOption Enumeration

NXOpen.Preferences.PartDrafting.UpdateViewWithoutLwDataOption is an alias for NXOpen.Preferences.PartDraftingUpdateViewWithoutLwDataOption

class NXOpen.Preferences.PartDraftingUpdateViewWithoutLwDataOption

Bases: object

Describes the update view without light weight data options

Enum Members

Enum Member Enum Member Description
Ignore
Ignore
Notify
Notify
DoNotNotify
Do Not Notify
Generate
Generate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.