ObjectPreferencesTranslucency Enumeration

NXOpen.Preferences.ObjectPreferences.Translucency is an alias for NXOpen.Preferences.ObjectPreferencesTranslucency

class NXOpen.Preferences.ObjectPreferencesTranslucency

Bases: object

Describes whether the translucency is enabled or disabled

Enum Members

Enum Member Enum Member Description
Disabled  
Enabled  
TemporarilyEnabled  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.