LoadDraftingStandardBuilderLoadLevel Enumeration¶
NXOpen.Preferences.LoadDraftingStandardBuilder.LoadLevel is an alias for NXOpen.Preferences.LoadDraftingStandardBuilderLoadLevel
-
class
NXOpen.Preferences.
LoadDraftingStandardBuilderLoadLevel
¶ Bases:
object
This enum is for the load level
Enum Members
Enum Member Enum Member Description Shipped the shipped levelPackage the package levelSite the site levelGroup the group levelUser the user level-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-