GeneralWireframeColorSourceOption Enumeration

class NXOpen.Preferences.GeneralWireframeColorSourceOption

Bases: object

Represents the wireframe color source options Enum Members

Enum Member Enum Member Description
FromBody
From Body
FromFace
From Face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.