GeneralToleranceOption Enumeration

class NXOpen.Preferences.GeneralToleranceOption

Bases: object

Represents the General tolerance options Enum Members

Enum Member Enum Member Description
Coarse
Coarse
Medium
Medium
Standard
Standard
Fine
Fine
ExtraFine
Extra Fine
Customize
Customize
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.