DetailBoundaryOption Enumeration

class NXOpen.Preferences.DetailBoundaryOption

Bases: object

Represents the boundary options Enum Members

Enum Member Enum Member Description
Circular
Circular boundary
Rectangular
Rectangular boundary
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.