NetworkObjectStatus Enumeration¶
NXOpen.Positioning.Network.ObjectStatus is an alias for NXOpen.Positioning.NetworkObjectStatus
-
class
NXOpen.Positioning.
NetworkObjectStatus
¶ Bases:
object
Specifies the solver status of a movable object.
Enum Members
Enum Member Enum Member Description Unknown Not yet evaluated.Fixed Attempt to put constraint between two fixed objects.OverDefined Conflicts with other constraints.NotConsistentDims Cannot solve with current dimension values. Model fully defined.NotConsistentOther Cannot find a solution. Model underdefined.NotConsistentUnknown One movable object fixed.NotChanged Not evaluated because other parts of the model are over defined or inconsistent.WellDefined The constraint is solved and satisfiedUnderDefined The constraint is solved and satisfied-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-