MatingConverterPartContext Enumeration¶
NXOpen.Positioning.MatingConverter.PartContext is an alias for NXOpen.Positioning.MatingConverterPartContext
-
class
NXOpen.Positioning.
MatingConverterPartContext
¶ Bases:
object
Defines in which parts mating conditions will be converted.
Enum Members
and all loaded children. Partially-loaded children will be fully-loaded. “
“InAllChildren”, ” Convert mating conditions in the owning partand all children. Partially-loaded and unloaded children will be fully-loaded. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-