ConstraintType Enumeration¶
NXOpen.Positioning.Constraint.Type is an alias for NXOpen.Positioning.ConstraintType
-
class
NXOpen.Positioning.
ConstraintType
¶ Bases:
object
Specifies the type of a constraint.
Enum Members
Enum Member Enum Member Description Undefined No typeTouch Two geometries touchConcentric Two geometries share a center and planeFix One movable object fixedDistance Two geometries have a specified distance between themParallel Two geometries are parallelPerpendicular Two geometries are perpendicularCenter12 One geometry is positioned mid-way between two othersCenter22 An implicit plane between two geometries of one movable object is positioned mid-way between two othersAngle Two geometries have a specified angle between themFit Two geometries are coincidentBond A number of movable objects form a rigid groupOrientAngle Two geometries have a specified angle between them about an axisSplineData A spline and its defining pointsSplineLength Constrains the curve length of a splineLinearPattern For internal use onlyCircularPattern For internal use onlyLinear2dPattern For internal use onlyRadiantPattern For internal use onlyAlignLock Two geometries are constrained to have a common axis and no rotation about itCommonOffsetTransform For internal use onlyJointHinge For internal use onlyJointSlider For internal use onlyJointCylindrical For internal use onlyJointBall For internal use onlyJointUniversal For internal use onlyJointPlanar For internal use onlyJointPointOnCurve For internal use only-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-