ConstraintSplineType Enumeration¶
NXOpen.Positioning.Constraint.SplineType is an alias for NXOpen.Positioning.ConstraintSplineType
-
class
NXOpen.Positioning.
ConstraintSplineType
¶ Bases:
object
Specifies how the spline points define the shape of the spline.
Enum Members
Enum Member Enum Member Description ByPoles Spline points define control points.ByPoints Spline points define interpolation/through points.Invalid Not a valid spline constraint.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-