ConstraintSolverStatus Enumeration¶
NXOpen.Positioning.Constraint.SolverStatus is an alias for NXOpen.Positioning.ConstraintSolverStatus
-
class
NXOpen.Positioning.
ConstraintSolverStatus
¶ Bases:
object
Specifies the status of a constraint.
Enum Members
Enum Member Enum Member Description NewlyCreated Not evaluated or suppressed since creationSuppressed Constraint is suppressedOutOfDate Needs evaluationOverConstrained Conflicts with other constraintsNotConsistentDims Cannot solve with current dimension values. Model fully definedNotConsistentOther Cannot find a solution. Model underdefinedNotConsistentUnknown Cannot find a solutionBetweenFixed Attempt to put constraint between two fixed objectsNotSolved Not evaluated because other parts of the model are over defined or inconsistentSolved The constraint is solved and satisfiedCannotSolve The constraint has invalid geometry and could not be passed to the solverDelayed The constraint is delayed and will not solveIgnoredInArrangement The current arrangement ignores all constraints and they will not solveInternallyInconsistent The constraint references invalid geometry for this constraint typeUnloadedGeometry The constraint could not solve as some geometry is unloadedPendingConvertedMc The constraint has been converted from a mating condition and has not solved since conversionConflictingWithWave The constraint has been suppressed because it’s conflicting with WAVEInconsistentLimits The constraint has limits that are inconsistent and it could not be passed to the solverBeyondLimits The value of the expression of the constraint is beyond its limits and it could not be passed to the solver-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-