ConstraintReferenceConstraintOrder Enumeration

NXOpen.Positioning.ConstraintReference.ConstraintOrder is an alias for NXOpen.Positioning.ConstraintReferenceConstraintOrder

class NXOpen.Positioning.ConstraintReferenceConstraintOrder

Bases: object

Specifies the order of the constraint reference used in a NXOpen.Positioning.Constraint.

Typically the order is set during creation, where the first constraint reference added is “outside” and the second “outside”. For Bond constraints, the order is set to be “unknown” at creation.

Enum Members

Enum Member Enum Member Description
Unknown
No order specified
Inside
Inside
Outside
Outside
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.