ConstraintAlignment Enumeration

NXOpen.Positioning.Constraint.Alignment is an alias for NXOpen.Positioning.ConstraintAlignment

class NXOpen.Positioning.ConstraintAlignment

Bases: object

Specifies alignment of directed geometries used in a constraint.

Enum Members

Enum Member Enum Member Description
InferAlign
Allow the solver to decide the alignment
CoAlign
Directions are the same
ContraAlign
Directions are opposite
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.