ComponentNetwork Class¶
-
class
NXOpen.Positioning.
ComponentNetwork
¶ Bases:
NXOpen.Positioning.Network
Network for use in positioning components in NX.
A component network extends the
NXOpen.Positioning.Network
by adding support for :py:class:`NXOpen.Assemblies.Arrangement`s.Use
NXOpen.Positioning.Positioner.EstablishNetwork()
to create an instance of this class.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DisplayComponent | Returns or sets the Assemblies.Component in which the display is changed by solving the network. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MoveObjectsState | Returns or sets the move objects state for the network. |
Name | Returns the custom name of the object. |
NetworkArrangementsMode | Returns or sets the arrangements mode for this network. |
NonMovingGroupGrounded | Returns or sets the grounded state of non-moving_group objects. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddConstraint | Add a Constraint to the network. |
AddMovableObject | Add a movable object to the network. |
ApplyToModel | Applies the current network state to the model. |
BeginDrag | Notify the network that a sequence of drag operations is about to begin. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DragByRay | Move objects which have been added to the network using Positioning.Network.AddMovableObject() . |
DragByTransform | Move objects which have been added to the network using Positioning.Network.AddMovableObject() . |
DragByTranslation | Move objects which have been added to the network using Positioning.Network.AddMovableObject() . |
EmptyMovingGroup | Remove all elements from the moving_group. |
EndDrag | Notify the network that a sequence of drag operations has ended. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMovableObjectStatus | Returns the solver status of a movable object. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
IsReferencedGeometryLoaded | Are the necessary objects loaded so that all connected constraints can be included during a drag or solve ? @return |
LoadReferencedGeometry | Load the necessary objects so that all connected constraints can be included during a drag or solve. |
Prints a representation of this object to the system log file. | |
RemoveAllConstraints | Remove all :py:class:`Constraint`s which have been explcitly added to the network. |
RemoveConstraint | Remove a Constraint from the network. |
RemoveMovableObject | Remove a movable object from the network. |
ResetDisplay | Returns the display objects to their model positions. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetMovingGroup | Set the elements of the moving_group. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Solve | Solves the constraint network. |
Enumerations¶
ComponentNetworkArrangementsMode Enumeration | Specifies how changes in the network are applied to arrangements. |
Property Detail¶
IsOccurrence¶
-
ComponentNetwork.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ComponentNetwork.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ComponentNetwork.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
NetworkArrangementsMode¶
-
ComponentNetwork.
NetworkArrangementsMode
¶ Returns or sets the arrangements mode for this network.
-------------------------------------
Getter Method
Signature
NetworkArrangementsMode()
Returns: The Positioning.ComponentNetworkArrangementsMode
.Return type: NXOpen.Positioning.ComponentNetworkArrangementsMode
New in version NX6.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
NetworkArrangementsMode(mode)
Parameters: mode ( NXOpen.Positioning.ComponentNetworkArrangementsMode
) – ThePositioning.ComponentNetworkArrangementsMode
.New in version NX6.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
OwningComponent¶
-
ComponentNetwork.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ComponentNetwork.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ComponentNetwork.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
ComponentNetwork.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
ComponentNetwork.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
ComponentNetwork.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.