ComponentConstraintGroupBuilder Class¶
-
class
NXOpen.Positioning.
ComponentConstraintGroupBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Positioning.ComponentConstraintGroupBuilder
builderTo create a new instance of this class, use
NXOpen.Assemblies.ComponentAssembly.CreateConstraintGroupBuilder()
Default values.
Property Value ConstraintCollectionType BetweenSelectedComponents RememberComponentState true New in version NX8.0.1.
Properties¶
Property | Description |
---|---|
ConstraintCollectionType | Returns or sets the constraint collection types |
ConstraintGroupName | Returns or sets the name of constraint group |
RememberComponentState | Returns or sets the toggle to remember selected component |
SelectedComponentList | Returns the selected components list |
SelectedConstraintsList | Returns the selected constraint list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetContextComponent | Gets the context component which is used to decide the displayed constraints that can be in the selected constraints list. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ConstraintCollectionType¶
-
ComponentConstraintGroupBuilder.
ConstraintCollectionType
¶ Returns or sets the constraint collection types
-------------------------------------
Getter Method
Signature
ConstraintCollectionType()
Returns: Return type: NXOpen.Positioning.ComponentConstraintGroupConstraintsCollectionType
New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
ConstraintCollectionType(constraintCollectionType)
Parameters: constraintCollectionType ( NXOpen.Positioning.ComponentConstraintGroupConstraintsCollectionType
) –New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ConstraintGroupName¶
-
ComponentConstraintGroupBuilder.
ConstraintGroupName
¶ Returns or sets the name of constraint group
-------------------------------------
Getter Method
Signature
ConstraintGroupName()
Returns: Return type: str New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
ConstraintGroupName(nameOfConstraintGroup)
Parameters: nameOfConstraintGroup (str) – New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
RememberComponentState¶
-
ComponentConstraintGroupBuilder.
RememberComponentState
¶ Returns or sets the toggle to remember selected component
-------------------------------------
Getter Method
Signature
RememberComponentState()
Returns: Return type: bool New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
RememberComponentState(rememberComponentState)
Parameters: rememberComponentState (bool) – New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SelectedComponentList¶
-
ComponentConstraintGroupBuilder.
SelectedComponentList
¶ Returns the selected components list
-------------------------------------
Getter Method
Signature
SelectedComponentList()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SelectedConstraintsList¶
-
ComponentConstraintGroupBuilder.
SelectedConstraintsList
¶ Returns the selected constraint list
-------------------------------------
Getter Method
Signature
SelectedConstraintsList()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
GetContextComponent¶
-
ComponentConstraintGroupBuilder.
GetContextComponent
¶ Gets the context component which is used to decide the displayed constraints that can be in the selected constraints list.
The context component is only set by the creator and can be None. If the context component is None the displayed constraints will be in same part as the constraint group.
Signature
GetContextComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX8.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Validate¶
-
ComponentConstraintGroupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.