MemberIdentifier Class¶
-
class
NXOpen.PartFamily.
MemberIdentifier
¶ Bases:
NXOpen.TransientObject
This class represents the unique identifier for a part family member.
It essentially consitiutes the FAM attr object and value pair. This object is to be used in lieu of member name, whenever a member is needed to be uniquely identified.
Use
PartFamily.TemplateManager.CreateMemberIdentifier()
to create a new member identifier.New in version NX10.0.0.
Method Detail¶
Dispose¶
-
MemberIdentifier.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector
Signature
Dispose()
New in version NX10.0.0.
License requirements: None.