FamilyAttributeAttrType Enumeration¶
NXOpen.PartFamily.FamilyAttribute.AttrType is an alias for NXOpen.PartFamily.FamilyAttributeAttrType
-
class
NXOpen.PartFamily.
FamilyAttributeAttrType
¶ Bases:
object
The part family attribute types.
These should always be in synch with the UF_fam_attr_types
New in version NX9.0.0.
Enum Members
Enum Member Enum Member Description Text text attributeNumeric numeric attributeInteger integer attributeDouble double attributeString string attributePart part attributeName name attributeInstance instance attributeExpression expression attributeMirror mirror attributeDensity density attributeFeature feature attributeMass asserted mass attributeMaterial material attributeUndefined undefined attribute type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-