OptimizationBuilderOptimizationTargetType Enumeration

NXOpen.Optimization.OptimizationBuilder.OptimizationTargetType is an alias for NXOpen.Optimization.OptimizationBuilderOptimizationTargetType

class NXOpen.Optimization.OptimizationBuilderOptimizationTargetType

Bases: object

Optimization type for objective

Enum Members

Enum Member Enum Member Description
Minimum
Target is minimum value of design objective
Maximum
Target is maximum value of design objective
Target
Target is specified value of design objective
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.