OptimizationBuilderOptimizationConvergenceSpeedType Enumeration

NXOpen.Optimization.OptimizationBuilder.OptimizationConvergenceSpeedType is an alias for NXOpen.Optimization.OptimizationBuilderOptimizationConvergenceSpeedType

class NXOpen.Optimization.OptimizationBuilderOptimizationConvergenceSpeedType

Bases: object

Convergence speed type

Enum Members

Enum Member Enum Member Description
Slow
Slow convergence speed
Medium
Medium convergence speed
Fast
Fast convergence speed
Infinite
Infinite convergence speed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.