OptimizationBuilderOptimizationAttributeType Enumeration

NXOpen.Optimization.OptimizationBuilder.OptimizationAttributeType is an alias for NXOpen.Optimization.OptimizationBuilderOptimizationAttributeType

class NXOpen.Optimization.OptimizationBuilderOptimizationAttributeType

Bases: object

Attribute type

Enum Members

Enum Member Enum Member Description
Expression
Expression attribute
KFAttribute
KF attribute
GeometryParameter
Geometry/feature parameter attribute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.