DesignStudyBuilderDesignStudyDistributeType Enumeration

NXOpen.Optimization.DesignStudyBuilder.DesignStudyDistributeType is an alias for NXOpen.Optimization.DesignStudyBuilderDesignStudyDistributeType

class NXOpen.Optimization.DesignStudyBuilderDesignStudyDistributeType

Bases: object

Distribution type

Enum Members

Enum Member Enum Member Description
Uniform
Uniform distribution type
Normal
Normal distribution type
Gamma
Gamma distribution type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.