VectorTorqueCollection Class¶
-
class
NXOpen.Motion.
VectorTorqueCollection
¶ Bases:
object
Represents a collection of vector torque objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateVectorTorqueBuilder | Creates a NXOpen.Motion.JointDriverBuilder @return |
FindObject | Finds the NXOpen.Motion.VectorTorque with the given name. |
Method Detail¶
CreateVectorTorqueBuilder¶
-
VectorTorqueCollection.
CreateVectorTorqueBuilder
¶ Creates a
NXOpen.Motion.JointDriverBuilder
Signature
CreateVectorTorqueBuilder(vectortorque)
Parameters: vectortorque ( NXOpen.Motion.VectorTorque
) – “NXOpen.Motion.VectorTorque
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.VectorTorqueBuilder
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
VectorTorqueCollection.
FindObject
¶ Finds the
NXOpen.Motion.VectorTorque
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.VectorTorque
.Returns: NXOpen.Motion.VectorTorque
with this name.Return type: NXOpen.Motion.VectorTorque
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)