TirePropertyMotorcycleCollection Class¶
-
class
NXOpen.Motion.
TirePropertyMotorcycleCollection
¶ Bases:
object
Represents a collection of Motion Motorcycle Tire Property elements
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateTirePropertyMotorcycleBuilder | Return NXOpen.Motion.TirePropertyMotorcycleBuilder object @return TirePropertyMotorcycleBuilder object |
FindObject | Finds the NXOpen.Motion.TirePropertyMotorcycle with the given name. |
Method Detail¶
CreateTirePropertyMotorcycleBuilder¶
-
TirePropertyMotorcycleCollection.
CreateTirePropertyMotorcycleBuilder
¶ Return
NXOpen.Motion.TirePropertyMotorcycleBuilder
objectSignature
CreateTirePropertyMotorcycleBuilder(tireProperty)
Parameters: tireProperty ( NXOpen.Motion.TirePropertyMotorcycle
) –NXOpen.Motion.TirePropertyMotorcycle
to be edited, if None then create a new oneReturns: TirePropertyMotorcycleBuilder object Return type: NXOpen.Motion.TirePropertyMotorcycleBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
TirePropertyMotorcycleCollection.
FindObject
¶ Finds the
NXOpen.Motion.TirePropertyMotorcycle
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.TirePropertyMotorcycle
Returns: NXOpen.Motion.TirePropertyMotorcycle
with this nameReturn type: NXOpen.Motion.TirePropertyMotorcycle
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)