TirePropertyHighOrderParameters Class¶
-
class
NXOpen.Motion.
TirePropertyHighOrderParameters
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Tire Property builder for the High Order parameters used in Motorcycle and Basic properties.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CarcassMass | Returns the carcass mass |
LateralDamping | Returns the lateral damping. |
LateralEffects | Returns or sets the lateral effects |
LateralStiffness | Returns the lateral stiffness. |
LongDamping | Returns the longitudinal damping |
LongStiffness | Returns the longitudinal stiffness |
LongitudinalEffects | Returns or sets the longitudinal effects |
RollMoment | Returns or sets the roll moment. |
Tag | Returns the Tag for this object. |
UnloadingVerticalStiffness | Returns or sets the unloading vertical stiffness. |
VerticalCarcassEffects | Returns or sets the vertical carcass effects |
VerticalStiffnessTransVelocity | Returns the vertical stiffness transitional velocity stiffness This parameter is only used in the Motion.TirePropertyBasic . |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CarcassMass¶
-
TirePropertyHighOrderParameters.
CarcassMass
¶ Returns the carcass mass
-------------------------------------
Getter Method
Signature
CarcassMass()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
LateralDamping¶
-
TirePropertyHighOrderParameters.
LateralDamping
¶ Returns the lateral damping.
This parameter is only used in the
Motion.TirePropertyBasic
.-------------------------------------
Getter Method
Signature
LateralDamping()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
LateralEffects¶
-
TirePropertyHighOrderParameters.
LateralEffects
¶ Returns or sets the lateral effects
-------------------------------------
Getter Method
Signature
LateralEffects()
Returns: Return type: bool New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
LateralEffects(inValue)
Parameters: inValue (bool) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
LateralStiffness¶
-
TirePropertyHighOrderParameters.
LateralStiffness
¶ Returns the lateral stiffness.
This parameter is only used in the
Motion.TirePropertyBasic
.-------------------------------------
Getter Method
Signature
LateralStiffness()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
LongDamping¶
-
TirePropertyHighOrderParameters.
LongDamping
¶ Returns the longitudinal damping
-------------------------------------
Getter Method
Signature
LongDamping()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
LongStiffness¶
-
TirePropertyHighOrderParameters.
LongStiffness
¶ Returns the longitudinal stiffness
-------------------------------------
Getter Method
Signature
LongStiffness()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
LongitudinalEffects¶
-
TirePropertyHighOrderParameters.
LongitudinalEffects
¶ Returns or sets the longitudinal effects
-------------------------------------
Getter Method
Signature
LongitudinalEffects()
Returns: Return type: bool New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
LongitudinalEffects(inValue)
Parameters: inValue (bool) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
RollMoment¶
-
TirePropertyHighOrderParameters.
RollMoment
¶ Returns or sets the roll moment.
This parameter is only used in the
Motion.TirePropertyBasic
. It is a flag that indicates whether or not the roll moment term introduced by the lateral spring-damper should be calculated. This roll moment is caused by the lateral displacement of the tire patch when a lateral spring-damper (lateral stiff) is included in the tire model. If cornering table or cornering stiffness are used, and roll moment is set to “True”, lateral stiffness is used to determine a lateral deflection that in turn is used to calculate a roll moment.-------------------------------------
Getter Method
Signature
RollMoment()
Returns: Return type: bool New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
RollMoment(inValue)
Parameters: inValue (bool) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
UnloadingVerticalStiffness¶
-
TirePropertyHighOrderParameters.
UnloadingVerticalStiffness
¶ Returns or sets the unloading vertical stiffness.
This parameter is only used in the
Motion.TirePropertyBasic
.-------------------------------------
Getter Method
Signature
UnloadingVerticalStiffness()
Returns: Return type: NXOpen.Motion.MotionFunction
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
UnloadingVerticalStiffness(func)
Parameters: func ( NXOpen.Motion.MotionFunction
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
VerticalCarcassEffects¶
-
TirePropertyHighOrderParameters.
VerticalCarcassEffects
¶ Returns or sets the vertical carcass effects
-------------------------------------
Getter Method
Signature
VerticalCarcassEffects()
Returns: Return type: bool New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
VerticalCarcassEffects(inValue)
Parameters: inValue (bool) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
VerticalStiffnessTransVelocity¶
-
TirePropertyHighOrderParameters.
VerticalStiffnessTransVelocity
¶ Returns the vertical stiffness transitional velocity stiffness This parameter is only used in the
Motion.TirePropertyBasic
.-------------------------------------
Getter Method
Signature
VerticalStiffnessTransVelocity()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
TirePropertyHighOrderParameters.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.