TirePropertyFtBuilder Class¶
-
class
NXOpen.Motion.
TirePropertyFtBuilder
¶ Bases:
NXOpen.Motion.TirePropertyBuilder
Represents a Builder for Motion Ftire Tire Property
To create a new instance of this class, use
NXOpen.Motion.TirePropertyFtCollection.CreateTirePropertyFtBuilder()
Default values.
Property Value IdRoad.Value 0 (millimeters part), 0 (inches part) Radius.Value 300.0 (millimeters part), 11.811 (inches part) RunInParallel 0 StaticHold 1 StaticVerticalStiffness.Value 0.0 (millimeters part), 0.0 (inches part) New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
FtireFile | Returns or sets the FTire file. |
IdRoad | Returns the IdRoad. |
Name | Returns or sets the name. |
Radius | Returns the Radius. |
RunInParallel | Returns or sets the run in parallel parameter. |
StaticHold | Returns or sets the static hold. |
StaticVerticalStiffness | Returns the static vertical stiffness. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FtireFile¶
-
TirePropertyFtBuilder.
FtireFile
¶ Returns or sets the FTire file.
This is a file containing information describing the FTire tire.
-------------------------------------
Getter Method
Signature
FtireFile()
Returns: Return type: str New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
FtireFile(fileName)
Parameters: fileName (str) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
IdRoad¶
-
TirePropertyFtBuilder.
IdRoad
¶ Returns the IdRoad.
It is a Road type identification number.
-------------------------------------
Getter Method
Signature
IdRoad()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Name¶
-
TirePropertyFtBuilder.
Name
¶ Returns or sets the name.
It is a uniqe name within tire properties.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Radius¶
-
TirePropertyFtBuilder.
Radius
¶ Returns the Radius.
It represents the undeformed radius of the tire.
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
RunInParallel¶
-
TirePropertyFtBuilder.
RunInParallel
¶ Returns or sets the “run in parallel” parameter.
This specifies if the FTire will automatically launch itself in parallel.
-------------------------------------
Getter Method
Signature
RunInParallel()
Returns: Return type: bool New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
RunInParallel(runInParallel)
Parameters: runInParallel (bool) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
StaticHold¶
-
TirePropertyFtBuilder.
StaticHold
¶ Returns or sets the static hold.
It controls holding forces during static analysis. These holding forces are applied to prevent tire spin and gross chassis motion (X and Y translation and yaw with respect to the road “up” vector).
-------------------------------------
Getter Method
Signature
StaticHold()
Returns: Return type: bool New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
StaticHold(staticHold)
Parameters: staticHold (bool) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
StaticVerticalStiffness¶
-
TirePropertyFtBuilder.
StaticVerticalStiffness
¶ Returns the static vertical stiffness.
It specifies the vertical stiffness only used in static equilibrating force calculations
-------------------------------------
Getter Method
Signature
StaticVerticalStiffness()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
TirePropertyFtBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.