TirePropertyCdCollection Class¶
-
class
NXOpen.Motion.
TirePropertyCdCollection
¶ Bases:
object
Represents a collection of Motion CDTire Tire Property elements
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateTirePropertyCdBuilder | Return NXOpen.Motion.TirePropertyCdBuilder object @return TirePropertyCdBuilder object |
FindObject | Finds the NXOpen.Motion.TirePropertyCd with the given name. |
Method Detail¶
CreateTirePropertyCdBuilder¶
-
TirePropertyCdCollection.
CreateTirePropertyCdBuilder
¶ Return
NXOpen.Motion.TirePropertyCdBuilder
objectSignature
CreateTirePropertyCdBuilder(tireProperty)
Parameters: tireProperty ( NXOpen.Motion.TirePropertyCd
) –NXOpen.Motion.TirePropertyCd
to be edited, if None then create a new oneReturns: TirePropertyCdBuilder object Return type: NXOpen.Motion.TirePropertyCdBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
TirePropertyCdCollection.
FindObject
¶ Finds the
NXOpen.Motion.TirePropertyCd
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.TirePropertyCd
Returns: NXOpen.Motion.TirePropertyCd
with this nameReturn type: NXOpen.Motion.TirePropertyCd
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)