TirePropertyCdBuilderModelType Enumeration¶
NXOpen.Motion.TirePropertyCdBuilder.ModelType is an alias for NXOpen.Motion.TirePropertyCdBuilderModelType
-
class
NXOpen.Motion.
TirePropertyCdBuilderModelType
¶ Bases:
object
The Model type.
See detailed documentation about each model type.
Enum Members
Enum Member Enum Member Description Cdt30 Cdt30Hps Cdt40 Cdt50 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-