TirePropertyAdvancedParametersRollingType Enumeration¶
NXOpen.Motion.TirePropertyAdvancedParameters.RollingType is an alias for NXOpen.Motion.TirePropertyAdvancedParametersRollingType
-
class
NXOpen.Motion.
TirePropertyAdvancedParametersRollingType
¶ Bases:
object
the rolling radius type.
When ‘None’ is selected a 0.0 value is exported for the Rolling Radius parameter. ‘Bias’ is used for a bias-ply tire and ‘Belted’ is for a belted radial tire.
Enum Members
Enum Member Enum Member Description NotSet Bias Belted -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-