SpringCollection Class¶
-
class
NXOpen.Motion.
SpringCollection
¶ Bases:
object
Represents a collection of motion spring
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateSpringBuilder | Return NXOpen.Motion.SpringBuilder object @return SpringBuilder object |
FindObject | Finds the NXOpen.Motion.Spring with the given name. |
Method Detail¶
CreateSpringBuilder¶
-
SpringCollection.
CreateSpringBuilder
¶ Return
NXOpen.Motion.SpringBuilder
objectSignature
CreateSpringBuilder(spring)
Parameters: spring ( NXOpen.Motion.Spring
) –NXOpen.Motion.Spring
to be edited, if None then create a new oneReturns: SpringBuilder object Return type: NXOpen.Motion.SpringBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
SpringCollection.
FindObject
¶ Finds the
NXOpen.Motion.Spring
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.Spring
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)