RoadBuilderSurfaceDatatypeChoices Enumeration¶
NXOpen.Motion.RoadBuilder.SurfaceDatatypeChoices is an alias for NXOpen.Motion.RoadBuilderSurfaceDatatypeChoices
-
class
NXOpen.Motion.
RoadBuilderSurfaceDatatypeChoices
¶ Bases:
object
data type attribute of the surface data
Enum Members
Enum Member Enum Member Description SplineCurve Spline CurveSplineSurface Spline SurfaceRsm1000 RSM1000Rsm1002 RSM1002Rsm2000 RSM2000Rsm3000 RSM3000OpenCRG OpenCRGRoadDataFile Road Data File-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-