ResultMeasureCollection Class¶
-
class
NXOpen.Motion.
ResultMeasureCollection
¶ Bases:
object
Represents a collection of result measure objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateResultMeasureBuilder | Creates a NXOpen.Motion.ResultMeasureBuilder . |
DeleteResultMeasures | Delete list of result measures. |
Find | Finds the NXOpen.Motion.ResultMeasure with the given name. |
UpdateResultMeasures | Update list of result measures. |
Method Detail¶
CreateResultMeasureBuilder¶
-
ResultMeasureCollection.
CreateResultMeasureBuilder
¶ Creates a
NXOpen.Motion.ResultMeasureBuilder
.If active
NXOpen.Motion.MotionSolution
is not present, builder will not be created.Signature
CreateResultMeasureBuilder(resultMeasure)
Parameters: resultMeasure ( NXOpen.Motion.ResultMeasure
) –NXOpen.Motion.ResultMeasure
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.ResultMeasureBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
DeleteResultMeasures¶
-
ResultMeasureCollection.
DeleteResultMeasures
¶ Delete list of result measures.
Signature
DeleteResultMeasures(resultMeasure)
Parameters: resultMeasure (list of NXOpen.Motion.ResultMeasure
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Find¶
-
ResultMeasureCollection.
Find
¶ Finds the
NXOpen.Motion.ResultMeasure
with the given name.An exception will be thrown if no object can be found with given name.
Signature
Find(name)
Parameters: name (str) – The name of the NXOpen.Motion.ResultMeasure
.Returns: NXOpen.Motion.ResultMeasure
with this name.Return type: NXOpen.Motion.ResultMeasure
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
UpdateResultMeasures¶
-
ResultMeasureCollection.
UpdateResultMeasures
¶ Update list of result measures.
Signature
UpdateResultMeasures(resultMeasure)
Parameters: resultMeasure (list of NXOpen.Motion.ResultMeasure
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)