PostProcess Class¶
-
class
NXOpen.Motion.
PostProcess
¶ Bases:
object
Represents the motion post process
To obtain an instance of this class, refer to
NXOpen.Motion.MotionSession
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CaptureArrangement | Capture or update an arrangement from motion result of active solution. |
CreateEnvelope | Creates envelopes for the given objects |
CreateSequence | Create sequence @return Sequence |
ExplodeMechanism | Explode mechanism @return NXOpen.Assemblies.Explosion |
ExportRealTimeMovie | Export a real-time movie |
ExportToMovie | Export to movie |
GetInterferenceOption | Get interference option for animation/articulation/spreadsheet run @return Interference on/off options |
GetMeasureOption | Get measure option animation/articulation/spreadsheet run @return Measure on/off options |
GetSpeed | Get the animation speed for motion animation @return The animation speed |
GetStopOnEventOption | Get stop on event option animation/articulation/spreadsheet run @return Stop on event on/off options |
GetTraceOption | Get trace option animation/articulation/spreadsheet run @return Trace on/off options |
ListInterference | List interference |
ListMeasure | List measure |
RegisterUserButton | Register user button for post process. |
SetInterferenceOption | Set interference option for animation/articulation/spreadsheet run |
SetMeasureOption | Set measure option animation/articulation/spreadsheet run |
SetSpeed | Set the animation speed for motion animation |
SetStopOnEventOption | Set articulation stop on event option animation/articulation/spreadsheet run |
SetTraceOption | Set articulation trace option animation/articulation/spreadsheet run |
TraceCurrentPosition | Trace current position |
TraceEntireMechanism | Trace entire mechanism |
TraceIntersectionCurve | Trace intersection curve |
UpdateDesignPosition | Update design position |
Enumerations¶
PostProcessEnvelopeAccuracyModes Enumeration | The modes for envelope accuracy |
PostProcessEnvelopeToleranceTypes Enumeration | Envelope tolerance types |
Structs¶
PostProcessEnvelopeTolerance_Struct Struct | Contains settings for envelope tolerance |
Method Detail¶
CaptureArrangement¶
-
PostProcess.
CaptureArrangement
¶ Overloaded method CaptureArrangement
CaptureArrangement(arrangementName, animationStep)
CaptureArrangement(arrangementName, arrangementType, animationStep)
-------------------------------------
Capture or update an arrangement from motion result of active solution. If an arrangement with the given name is present, updates the arrangement. Otherwise new arrangement of the standard type is created.
Signature
CaptureArrangement(arrangementName, animationStep)
Parameters: - arrangementName (str) – Name for arrangement
- animationStep (int) – Animation step
Returns: Assembly arrangement
Return type: New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Capture or update an arrangement from motion result of active solution. If an arrangement with the given name is present, updates the arrangement. The arrangement type cannot be changed during update. If an arrangement with the given name is not present, new arrangement is created. The new arrangement could be isolated or standard type. It depends on the arrangementType argument
Signature
CaptureArrangement(arrangementName, arrangementType, animationStep)
Parameters: - arrangementName (str) – Name for arrangement
- arrangementType (int) – Arrangement type
- animationStep (int) – Animation step
Returns: Assembly arrangement
Return type: New in version NX9.0.1.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
CreateEnvelope¶
-
PostProcess.
CreateEnvelope
¶ Creates envelopes for the given objects
Signature
CreateEnvelope(tPostControl, destinationPart, addToRefSets, referenceFrameObj, sourceObjs, stepFrom, stepTo, toleranceSetting)
Parameters: - tPostControl (
NXOpen.Motion.IPostControl
) – The IPostControl object - destinationPart (
NXOpen.NXObject
) – The part to save swept the objects into - addToRefSets (bool) – Indicates whether the output should be added to Model/Lightweight reference sets or not
- referenceFrameObj (
NXOpen.NXObject
) – The object acts as reference frame - sourceObjs (list of
NXOpen.NXObject
) – The objects swept bodies are created from - stepFrom (int) – The step index where the envelope starts
- stepTo (int) – The step index where the envelope stops
- toleranceSetting (
NXOpen.Motion.PostProcessEnvelopeTolerance_Struct
) – The tolerance settings
Returns: a tuple
Return type: A tuple consisting of (sweptBodies, skipedObj, failedObjs, aborted). sweptBodies is a list of
NXOpen.NXObject
. The resulting swept bodies skipedObj is a list ofNXOpen.NXObject
. The objects skipped because invisible or not moving failedObjs is a list ofNXOpen.NXObject
. The objects failed because of an algorithm failure aborted is a bool. True if user hits the stop button, false otherwiseNew in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
- tPostControl (
CreateSequence¶
-
PostProcess.
CreateSequence
¶ Create sequence
Signature
CreateSequence(sequenceName)
Parameters: sequenceName (str) – The sequence name Returns: Sequence Return type: NXOpen.NXObject
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
ExplodeMechanism¶
-
PostProcess.
ExplodeMechanism
¶ Explode mechanism
Signature
ExplodeMechanism(explosionName)
Parameters: explosionName (str) – Name for explosion Returns: NXOpen.Assemblies.Explosion
Return type: NXOpen.Assemblies.Explosion
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
ExportRealTimeMovie¶
-
PostProcess.
ExportRealTimeMovie
¶ Export a real-time movie
Signature
ExportRealTimeMovie(movieName)
Parameters: movieName (str) – Name for movie to export New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
ExportToMovie¶
-
PostProcess.
ExportToMovie
¶ Export to movie
Signature
ExportToMovie(movieName)
Parameters: movieName (str) – Name for movie to export New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetInterferenceOption¶
-
PostProcess.
GetInterferenceOption
¶ Get interference option for animation/articulation/spreadsheet run
Signature
GetInterferenceOption()
Returns: Interference on/off options Return type: bool New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetMeasureOption¶
-
PostProcess.
GetMeasureOption
¶ Get measure option animation/articulation/spreadsheet run
Signature
GetMeasureOption()
Returns: Measure on/off options Return type: bool New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetSpeed¶
-
PostProcess.
GetSpeed
¶ Get the animation speed for motion animation
Signature
GetSpeed()
Returns: The animation speed Return type: int New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetStopOnEventOption¶
-
PostProcess.
GetStopOnEventOption
¶ Get stop on event option animation/articulation/spreadsheet run
Signature
GetStopOnEventOption()
Returns: Stop on event on/off options Return type: bool New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetTraceOption¶
-
PostProcess.
GetTraceOption
¶ Get trace option animation/articulation/spreadsheet run
Signature
GetTraceOption()
Returns: Trace on/off options Return type: bool New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
ListInterference¶
-
PostProcess.
ListInterference
¶ List interference
Signature
ListInterference()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
ListMeasure¶
-
PostProcess.
ListMeasure
¶ List measure
Signature
ListMeasure()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
RegisterUserButton¶
-
PostProcess.
RegisterUserButton
¶ Register user button for post process.
If the functionBeforeUIDestroy is register, the motion post animation, articulation, spreadsheet run UI will display the user button as the buttonName and buttonTips setting. and in this button action, it will invoke the register function and the function by menu script registered
Signature
RegisterUserButton(buttonName, buttonTips, buttonMenuScriptName, functionBeforeUIDestroy)
Parameters: - buttonName (str) – the name displayed on the button
- buttonTips (str) – the button tool tip
- buttonMenuScriptName (str) – the menu script name of the button
- functionBeforeUIDestroy (CallableObject) – User function for this button before dialog destroy
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetInterferenceOption¶
-
PostProcess.
SetInterferenceOption
¶ Set interference option for animation/articulation/spreadsheet run
Signature
SetInterferenceOption(interferenceOn)
Parameters: interferenceOn (bool) – Interference on/off options New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetMeasureOption¶
-
PostProcess.
SetMeasureOption
¶ Set measure option animation/articulation/spreadsheet run
Signature
SetMeasureOption(measureOn)
Parameters: measureOn (bool) – Measure on/off options New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetSpeed¶
-
PostProcess.
SetSpeed
¶ Set the animation speed for motion animation
Signature
SetSpeed(speed)
Parameters: speed (int) – The animation speed New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetStopOnEventOption¶
-
PostProcess.
SetStopOnEventOption
¶ Set articulation stop on event option animation/articulation/spreadsheet run
Signature
SetStopOnEventOption(stopOnEventOn)
Parameters: stopOnEventOn (bool) – Stop on event on/off options New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetTraceOption¶
-
PostProcess.
SetTraceOption
¶ Set articulation trace option animation/articulation/spreadsheet run
Signature
SetTraceOption(traceOn)
Parameters: traceOn (bool) – Trace on/off options New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
TraceCurrentPosition¶
-
PostProcess.
TraceCurrentPosition
¶ Trace current position
Signature
TraceCurrentPosition()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
TraceEntireMechanism¶
-
PostProcess.
TraceEntireMechanism
¶ Trace entire mechanism
Signature
TraceEntireMechanism()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)