PortVariable Class¶
-
class
NXOpen.Motion.
PortVariable
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
Motion.PortVariable
.This class contains the port association for the output of a mechatronics element No KF support
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AssociatedPortName | Returns or sets the associated port name |
Name | Returns the name |
Port | Returns the port |
Tag | Returns the Tag for this object. |
Unit | Returns the unit |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssociatedPortName¶
-
PortVariable.
AssociatedPortName
¶ Returns or sets the associated port name
-------------------------------------
Getter Method
Signature
AssociatedPortName()
Returns: Return type: str New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
AssociatedPortName(associatedPortName)
Parameters: associatedPortName (str) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Name¶
-
PortVariable.
Name
¶ Returns the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Port¶
-
PortVariable.
Port
¶ Returns the port
-------------------------------------
Getter Method
Signature
Port()
Returns: Return type: NXOpen.Motion.ControlPort
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
PortVariable.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.