PointOnCurveCollection Class¶
-
class
NXOpen.Motion.
PointOnCurveCollection
¶ Bases:
object
Represents a collection of point on curve objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreatePointOnCurveBuilder | Creates a NXOpen.Motion.PointOnCurveBuilder @return |
FindObject | Finds the NXOpen.Motion.PointOnCurve with the given name. |
Method Detail¶
CreatePointOnCurveBuilder¶
-
PointOnCurveCollection.
CreatePointOnCurveBuilder
¶ Creates a
NXOpen.Motion.PointOnCurveBuilder
Signature
CreatePointOnCurveBuilder(pointOnCurve)
Parameters: pointOnCurve ( NXOpen.Motion.PointOnCurve
) –NXOpen.Motion.PointOnCurve
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.PointOnCurveBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
PointOnCurveCollection.
FindObject
¶ Finds the
NXOpen.Motion.PointOnCurve
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.PointOnCurve
.Returns: NXOpen.Motion.PointOnCurve
with this name.Return type: NXOpen.Motion.PointOnCurve
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)